Hi all, I went to a Freescale wireless seminar in Michigan about a year ago. We used a small demo board in the lab tests and I am having a difficult time locating that demo board on the Freescale site. I think the demo board has both an 8 bit MPU and the wireless chip on it. Basically, I only need to run a simple field test in a factory for range and dead spots. The resulting functionality I will need is to send 1-4 bytes of data to a mobile cart using wireless. So, I have a few questions for the group: 1. What is that demo board part number and is it available? 2. Can I just use the wireless chips in a "test mode" where just the "carrier" is transmitted to a receiver and do something like light up a LED if signal is present? 3. Any other suggestions on making a simple site test?
The MC13192DSK might be the demo we used, but I thought it had a USB connector on it. Also, thanks for the link to the range testing information. I will check the datasheet to see if I can run a test with just the radio, but no MPU. Thanks, David