Marco Stevanoni

Clock Sources on MC1321x

Discussion created by Marco Stevanoni on Feb 15, 2007
Latest reply on Feb 16, 2007 by Marco Stevanoni
Is it possible to connect both clock source on MC1321x
in order to use 16MHz when radio modem is on, and 32kHz when
I switch off the radio and run only the S08 micro section?

To obtain ultra low power, I need to switch on the radio modem
only when I need, but I need a S08 section running without
using internal (not exact) clock sources.

Stevasway

Outcomes