iMX515 Chinese Tablet PC - usb hub error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX515 Chinese Tablet PC - usb hub error

1,153 Views
RizalAbdurrahma
Contributor I

Dear, All

 

i Got iMX515 Chinese Tablet PC,aka Herotab M802, powered android and IMX515. After weeks playing with this tabled, time to do somethink fun, i found the design inside this Tablet is based on IMX515 EVKJ. Found this chip inside :

SC/GTL50/800  SGTL5000
MCIMX515DJM8C
MC13892JVL
MMA7660
AR6102G-BM2D
NT5TU64M16GG-AC
USB2514B                                   4 Port USB HUB
BT425183S KD12 2000mAh
ETRONTECH eSP258E                 USB CAMERA
HLY080MI                                    24 Bit 800x600 LCD

 

I have successfully installed lucid_1108 on it but,the problem is, usb hub not detected. Seem on kernel load process, my mouse whose attached to the hub is shortly lighting (Powering ON) but then shut it off.

 

trying dmesg on hacked mx tty uart tespoint inside give me :

 

CPU: ARMv7 Processor [412fc085] revision 5 (ARMv7), cr=10c53c7f
CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
Machine: Freescale MX51 Babbage Board
Memory policy: ECC disabled, Data cache writeback
On node 0 totalpages: 106496
free_area_init_node: node 0, pgdat 806d98fc, node_mem_map 8070a000
  DMA zone: 192 pages used for memmap
  DMA zone: 0 pages reserved
  DMA zone: 24384 pages, LIFO batch:3
  Normal zone: 640 pages used for memmap
  Normal zone: 81280 pages, LIFO batch:15
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 105664
Kernel command line: console=ttymxc0,115200 video=mxcdi1fb:800x600M-16@60 di1_primary console=tty0 root=/dev/mmcblk0p1 rootwait rw
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 416MB = 416MB total
Memory: 415060k/415060k available, 10924k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    DMA     : 0xf9e00000 - 0xffe00000   (  96 MB)
    vmalloc : 0x9a800000 - 0xf4000000   (1432 MB)
    lowmem  : 0x80000000 - 0x9a000000   ( 416 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .init : 0x80008000 - 0x8002f000   ( 156 kB)
      .text : 0x8002f000 - 0x80672000   (6412 kB)
      .data : 0x8068e000 - 0x806da780   ( 306 kB)
SLUB: Genslabs=11, HWalign=32, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
        RCU-based detection of stalled CPUs is disabled.
        Verbose stalled-CPUs detection is disabled.
NR_IRQS:368
MXC GPIO hardware
MXC IRQ initialized
MXC_Early serial console at MMIO 0x73fbc000 (options '115200')
bootconsole [ttymxc0] enabled
Console: colour dummy device 80x30
console [tty0] enabled, bootconsole disabled
Calibrating delay loop... 799.53 BogoMIPS (lpj=3997696)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
regulator: core version 0.5
NET: Registered protocol family 16
i.MX IRAM pool: 128 KB@0x9a840000
IRAM READY
CPU is i.MX51 Revision 3.0
Using SDMA I.API
MXC DMA API initialized
bio: create slab <bio-0> at 0
SCSI subsystem initialized
CSPI: mxc_spi-0 probed
Freescale USB OTG Driver loaded, $Revision: 1.55 $
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
MXC HS I2C driver
IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
PMIC Light driver loading...
Advanced Linux Sound Architecture Driver Version 1.0.23.
Bluetooth: Core ver 2.15
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
mc13892 Rev 2.0 FinVer 2 detected
Initializing regulators for Babbage.
regulator: SW1: 600 <--> 1375 mV at 1050 mV
regulator: SW2: 900 <--> 1850 mV at 1225 mV
regulator: SW3: 1100 <--> 1850 mV at 1200 mV
regulator: SW4: 1100 <--> 1850 mV at 1800 mV
regulator: SWBST:
regulator: VIOHI:
regulator: VPLL: 1050 <--> 1800 mV at 1800 mV
regulator: VDIG: 1650 mV
regulator: VSD: 1800 <--> 3150 mV at 3150 mV
regulator: VUSB2: 2400 <--> 2775 mV at 2600 mV
regulator: VVIDEO: 2775 mV
regulator: VAUDIO: 2300 <--> 3000 mV at 3000 mV
regulator: VCAM: 2500 <--> 3000 mV at 2600 mV fast normal
regulator: VGEN1: 1200 mV
regulator: VGEN2: 1200 <--> 3150 mV at 3150 mV
regulator: VGEN3: 1800 <--> 2900 mV at 1800 mV
regulator: VUSB:
regulator: GPO1:
regulator: GPO2:
regulator: GPO3:
regulator: GPO4:
PMIC ADC start probe
PMIC Light successfully loaded
Device spi1.0 probed
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
TCP established hash table entries: 16384 (order: 5, 131072 bytes)
TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
LPMode driver module loaded
Static Power Management for Freescale i.MX5
PM driver module loaded
sdram autogating driver module loaded
Bus freq driver module loaded
DI1 is primary
mxc_dvfs_core_probe
DVFS driver module loaded
i.MXC CPU frequency driver
DVFS PER driver module loaded
JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 810
alg: No test for stdrng (krng)
cryptodev: driver loaded.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
fbcvt: 800x600@60: CVT Name - .480M3
mxc_ipu mxc_ipu: Channel already disabled 9
mxc_ipu mxc_ipu: Channel already uninitialized 9
Console: switching to colour frame buffer device 100x37
fbcvt: 1024x768@60: CVT Name - .786M3
mxci2c_wait_writefifo:wait error
sii9022 3-0039: SII9022: cound not find device
regulator: get() with no identifier
regulator: get() with no identifier
regulator: get() with no identifier
mxci2c_wait_writefifo:wait error
Serial: MXC Internal UART driver
mxcintuart.0: ttymxc0 at MMIO 0x73fbc000 (irq = 31) is a Freescale i.MX
console [ttymxc0] enabled
mxcintuart.1: ttymxc1 at MMIO 0x73fc0000 (irq = 32) is a Freescale i.MX
mxcintuart.2: ttymxc2 at MMIO 0x7000c000 (irq = 33) is a Freescale i.MX
loop: module loaded
mxc_dataflash spi1.1: JEDEC id 000000 not handled
MXC MTD nand Driver 3.0
i.MX GPMI NFC
vcan: Virtual CAN interface driver
Freescale FlexCAN Driver
FEC Ethernet Driver
fec_enet_mii_bus: probed
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 18, io base 0x73f80000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 14, io base 0x73f80200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
ARC USBOTG Device Controller driver (1 August 2005)
mice: PS/2 mouse device common for all mice
MXC keypad loaded
input: mxckpd as /devices/virtual/input/input0
mc13892 rtc probe start
pmic_rtc pmic_rtc.1: rtc core: registered pmic_rtc as rtc0
mc13892 rtc probe succeed
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
Linux video capture interface: v2.00
mxc_v4l2_output mxc_v4l2_output.0: Registered device video0
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v0.1.0)
APM Battery Driver
MXC WatchDog Driver 2.0
MXC Watchdog # 0 Timer: initial timeout 60 sec
Bluetooth: Virtual HCI driver ver 1.3
Bluetooth: Generic Bluetooth USB driver ver 0.6
usbcore: registered new interface driver btusb
pmic_battery: probe of pmic_battery.1 failed with error -1
VPU initialized
mxsdhci: MXC Secure Digital Host Controller Interface driver
mxsdhci: MXC SDHCI Controller Driver.
mmc0: SDHCI detect irq 128 irq 1 INTERNAL DMA
mxsdhci: MXC SDHCI Controller Driver.
usb 2-1: new high speed USB device using fsl-ehci and address 2
mmc1: SDHCI detect irq 134 irq 2 INTERNAL DMA
Registered led device: pmic_ledsr
Registered led device: pmic_ledsg
Registered led device: pmic_ledsb
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
Cirrus Logic CS42888 ALSA SoC Codec Driver
sgtl5000-i2c 1-000a: SGTL5000 revision 17
No device for DAI imx-ssi-1-0
No device for DAI imx-ssi-1-1
No device for DAI imx-ssi-2-0
No device for DAI imx-ssi-2-1
No device for DAI imx-ssi-3-0
No device for DAI imx-ssi-3-1
DMA Sound Buffers Allocated:UseIram=1 buf->addr=1fff6000 buf->area=9a856000 size=24576
DMA Sound Buffers Allocated:UseIram=1 buf->addr=a92a8000 buf->area=fa2fa000 size=24576
asoc: SGTL5000 <-> imx-ssi-2-0 mapping ok
hub 2-1:1.0: USB hub found
hub 2-1:1.0: 4 ports detected
mmc0: new SDHC card at address e624
mmcblk0: mmc0:e624 SU04G 3.69 GiB
 mmcblk0: p1
ALSA device list:
  #0: imx-3stack (SGTL5000)
TCP cubic registered
NET: Registered protocol family 17
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
Bluetooth: L2CAP ver 2.14
Bluetooth: L2CAP socket layer initialized
Bluetooth: SCO (Voice Link) ver 0.6
Bluetooth: SCO socket layer initialized
Bluetooth: RFCOMM TTY layer initialized
Bluetooth: RFCOMM socket layer initialized
Bluetooth: RFCOMM ver 1.11
Bluetooth: BNEP (Ethernet Emulation) ver 1.3
Bluetooth: BNEP filters: protocol multicast
Bluetooth: HIDP (Human Interface Emulation) ver 1.2
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 2
USB Host suspend begins
will suspend roothub and its children
ehci_fsl_bus_suspend, DR
host suspend ends
regulator_init_complete: disabling VCAM
regulator_init_complete: disabling VAUDIO
regulator_init_complete: disabling VSD
input: mxc_ts as /devices/virtual/input/input1
mxc input touchscreen loaded
pmic_rtc pmic_rtc.1: setting system clock to 1970-01-02 04:26:46 UTC (102406)
mmc1: queuing unknown CIS tuple 0x01 (3 bytes)
EXT3-fs: barriers not enabled
kjournald starting.  Commit interval 5 seconds
mmc1: queuing unknown CIS tuple 0x1a (5 bytes)
mmc1: queuing unknown CIS tuple 0x1b (8 bytes)
mmc1: queuing unknown CIS tuple 0x14 (0 bytes)
EXT3-fs (mmcblk0p1): using internal journal
EXT3-fs (mmcblk0p1): mounted filesystem with writeback data mode
VFS: Mounted root (ext3 filesystem) on device 179:1.
Freeing init memory: 156K
mmc1: queuing unknown CIS tuple 0x80 (1 bytes)
mmc1: queuing unknown CIS tuple 0x81 (1 bytes)
mmc1: queuing unknown CIS tuple 0x82 (1 bytes)
mmc1: new SDIO card at address 0001
hub 2-1:1.0: hub_port_status failed (err = -110)
hub 2-1:1.0: hub_port_status failed (err = -110)
mxc_ipu mxc_ipu: Channel already disabled 9
mxc_ipu mxc_ipu: Channel already uninitialized 9
hub 2-1:1.0: hub_port_status failed (err = -110)
hub 2-1:1.0: hub_port_status failed (err = -110)
ehci_fsl_bus_resume, DR

 

============

 

Please if anyone can help me,about how to enabled the usb-hub. Official android (froyo)  was able to acces usb keyboard. Thanks.

 

Regards,

 

Rijal

Tags (1)
0 Kudos
0 Replies