YuLin YuLin

4 Camera input, vpu encode and image processing, is i.mx53 capable?

Discussion created by YuLin YuLin on Jul 1, 2011
Latest reply on Jun 20, 2012 by Jason Shi

I am searching a hardware solution for the follow requirement:

1. 4 camera input, resolution 640*480. NTSC or PAL

2. The above 4 camera input will be encode with VPU h264 into SD Card.

3. At the same time, these 4 frames will be processed by a simpel image function.

 

According to reference for i.mx53, it can process up to 4 encode/decode work simultaneously.

 

i.mx53 can afford to this work, is it right?

Outcomes