Hey all,
I have been working on my custom board with imx233. During the boared design, I made some imx pins (as GPIO) to control other components on board.
The imx wiki page has all the instruction on how to use GPIOs in the user space on the following link:
http://www.imxdev.org/wiki/index.php?title=FAQ_ALL_BOARDS_GPIO_TEST
But there is no option, or I can't see, in LTIB config that allows to configure SYSFS
I mean I can't see this
Device Drivers ---> --- GPIO Support [*] /sys/class/gpio/... (sysfs interface) as mentioned in the wiki so, how do I configure LTIB to export GPIO thru SYSFS?
I had the syntax wrong, by the way. Try:
%http_proxy
%gpp_proxy
1
If this still doesn't work, post your .ltibrc here. Also, can you ping bitshrine.org? Does network connectivity still fail if you do: ./ltib --dltest
Hi Daniel,
Did you add these two lines to .ltibrc:
%http_proxy=proxy.server:port
%proxy=1
Mariano
Thank you guys,
Another problem is, LTIB can't download packages either from the GPP or PPP; it always reports "No network connection is available to download.." I tried to edit the proxy in .ltibrc, but didn't help
can you tell me how can I enable LTIB to access the PPP/GPP. I'm using proxy to connect to the Internet
Daniel,
Mariano is correct. This is a kernel configuration option.
Regards,
Fabio Estevam
Hi Daniel,
I haven't double checked this (I will in a few hours if this doesn't help you), but I believe that's a kernel option. So to change that, in LTIB you'd need to check the box to re-configure the kernel.
Then once LTIB starts building, it'll bring up the kernel menuconfig, and then you'll be able to find this option there.
Mariano