AnsweredAssumed Answered

I can't set up break points in the source editor(code worrior 5.0)

Question asked by Harry Sun on Jan 23, 2007
Latest reply on Jan 24, 2007 by Joerg Schnyder
anybody can help? please,I can't set up break points in the source editor(code worrior 5.0),I can only do this in the debugger
 
when I click on the left-most column on the line on which I want to break,a red dot indeed appears, but it doesn't stop in the debugger.
I tried to seek some info in the help menu and found that it say i miss the DAC programm which is said being included in the installation disks under "addons" directory. However, I searched all the disks ,I thaven't found this file,though I indeed found the addons directory.
 
please help solve the problem, this feature is very convient and I need this.
 
thanks a million.
 
Harry
 

Outcomes