USB WiFi dongles

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB WiFi dongles

692 Views
PeteSwenson
Contributor I

Has anyone tested or know of any working USB WiFi dongles with the QSB?  There appears to be support for Atheros, but I don't know to what extent.

 

I've plugged in the following, but they didn't come up:

 

Linksys WUSB300N

Rosewill RNX-G1

TP-LINK TL-WN321G

 

Thanks.

Labels (1)
0 Kudos
1 Reply

498 Views
CraigPetku
Contributor III

I enabled the dlink DWA-160A2 (under $20 on ebay) under Android a couple weeks back on an EVK derivative.  Should work on the QSB as well.  The biggest trick is WPA supplicant.  If I have some time I'll try to post a clean patch for the QSB Ubuntu as well, but you may find the attached a little helpful.  The driver is compiled as a .ko as part of the kernel build then manually copied to a prebuilt folder along with the firmware files.

0 Kudos