Julian Rodrigues

Target settings

Discussion created by Julian Rodrigues Employee on Jan 15, 2007
Latest reply on Jan 17, 2007 by CrasyCat
Hi,
    I have projects for 2 targets(7119 and 8101) in a  directory and want to run the project for the targets on a machine where these two target boards are connected.The issue is that since both the target boards are connected to the PC using individual  USB TAP's when I debug say 7119 project am not able to download the executable to the board.Is there any way out where I could download the executable to the appropriate board when debugged.
 
Thanks

Outcomes