Hi,
Thanks for the reply Paolo.
I have already read the MCF5329 Reference Manual and the MCF5329 Hardware Specification and
I have set the flex-bus for accessing Compact Flash in this way:
CSAR1 = 0x02000000;
CSCR1 = 0x002A3780; //as MCF5329 Hardware Specification
CSMR1 = 0x01FF0001; // Compact Flash with 32MB of memory
I have try to write from the 0x02000000 address but I can't.
Have I to set something else?
Thank you very much,
mastro