Hey
I'm using a P&E MultiLink debugger for my ColdFire project, debuggin my current project executing from address 0 in FLASH, as a normal project.
The thing is, that I have this Bootloader, that I would like place in the start of the FALSH.
I have tried to move the start address of the application (that the Bootloader in the end should load) in my linker file with out any luck.
rom (RX) : ORIGIN = 0x00007800, LENGTH = 0x00018700
I would like to debug eaven though the start address is not 0.
What other changes do I have to make to my application project to make it execute.
Any guide lines?