Hi everyone,
I start a new design with I.MX51. I'm looking for an embedded Wi-Fi module on my board.
I saw the RS9110-N-11-26 from "Redpine signals". I'm looking for something like that but this one has max 65Mbps.
I would like 802.11abgn with 150Mbps max.
Any suggestion?
Thx, Maxime
Hey Max,
As far I read in datasheet of RS9110-N-22-01, which could be your second option, Redpine does not charge for license... The N-22-01 is open firm-ware ready to work.
I just catch up your answer.
The best option we found - so far - is the module RS9110-N-11-03. We don't want to use a chipset, we prefer to go with a module for a couple of reasons...
We are actually dealing with Redpine regarding the expensive annual license for using their products... I'll let you know.
Thanks, Max
Does it have to be a module? The Redpine Signals RS9116 does 150mbps and has an SDIO interface so it can interface to the i.MX51.
Thx Rick,
Their max bit rate is 54Mbps. Thx anyway.
Max
Not sure what their bit rates are, but check out http://www.wi2wi.com/.