Message Edited by peg on 2006-12-2709:15 PM
Hi,
I downloaded some firmware such as Test Mode App on your website and I also have a reference design MC13213SRB module. Also, I have my own project using mc13213 same design as with reference only without some peripherals (USB,Serial and memory). The difference is that my design is single ended (rf front-end) as compared with the reference its double ended (external switch). The test mode app configured for external switch. I would like to use the internal switch for test mode app.
What will I edit in the test mode app program (see attached file.)? I need to transfer the PA from PA1 to PA2.
I edited the MC13192_hw_config.c
SPIDrvWrite(0x07,0x0B80); /* Enable CLKo in Doze */
What else should I edit to tranform the firmware to single ended RF (Internal switch)?
THanks,
Allen RUbis