Slow throughput for MC13213 SRB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Slow throughput for MC13213 SRB

1,188 Views
thngkl
Contributor I
I am using the MC13213 SRB for my project and i am using the packet mode for transmitting and receiving. The input to the transmitting side is a 11 bit data and new data arrives every 1ms. The SRB is supposed to send these data to the receiving side. However i realise that the throughput is too slow, meaning that the transmitter is not fast enough to process and send the data out every 1ms. What do i need to change in order to increase the processing speed?
Labels (1)
0 Kudos
1 Reply

252 Views
NLFSJ
Contributor III
I am not very familiar with the device, but as the MC13213 reference manual say, the maximum throughput is 250 kbps. It means that the baudrate will depend on the amount of bytes that the application is transmitting, the data processing and the codification of the application. Unfortunately there is nothing to do in order to enhance the SMAC broadcast speed. Remember the MC13213 system is intended to monitoring and control application with a low baudrate needed.
 
Regards,
Nina
0 Kudos