Hello,
I'm currently working on my own BDM communication module from one S12X to another...
The protocol works fine, until now I can read and write on-chip registers and the RAM area.
But I'm a little bit confused about the WRITE_BYTE and WRITE_BD_BYTE commands.
In the document they are described as following:
>> Write to memory with standard BDM firmware lookup table in map.
>> Odd address data on low byte; even address data on high byte.
So what should I do to write a single byte without affecting its neighbour?
Thanks in advance,
-> pittbull