Hello
I would not recommend using make file importer wizard.
I would suggest you to proceed as follows:
- Create a project for the board you are targeting using the project wizard.
If you do not find it, just pick up the closest architecture.
- Remove the file main.c from the newly created project and add your project source files to the project.
- Check which were the options needed in the make file and add them to your project
- eventually adjust the linker command file
This should be working.
CrasyCat