Harjit Singh

Coldfire: Q on latest CodeWarrior Special Edition debug support

Discussion created by Harjit Singh on Dec 5, 2006
Latest reply on Dec 7, 2006 by Harjit Singh
Does it support Coldfire with the ICD Cable. The ICD cable is a BDM cable that plugs into the parallel port and has a 10 pin connector (0.1", 2x5).
 
I use this with SingleStep and a 68376 and wanted to know if I could use this cable on a MCF5212 design.
 
Also, does CodeWarrior Special Edition come with a ROM based monitor that I can use with CodeWarrior so that I can debug over the serial port?
 
Thanks,
Harjit

Message Edited by CrasyCat on 2007-04-13 11:30 AM

Outcomes