Solved! Go to Solution.
Dear Tom
the case is simple. I want to create a new project for the HCS908AW16, to built my OS for this type of MCU. Normally this is simple (i have done this for about 50 times) choosing the project wizard. But in this case the AW16 is still missing in the list (AW32, 48, 64) are the only choice. Choosing i.e. the AW32 for the project creates problems with the wrong MCU ID. So updating the project wizard for the AW16 would be great.
The board is one of my modules for the HC(S) system. See under www.systech-gmbh.ch -> HC(S) System.
Thanks a lot
Joerg
Dear Joerg,
I don't quite understand the dates here, as your question here is from JAN 15, but all others are from 2006???
Anyhow, if you still need a solution, I built several projects with the AW16. I built them using the AW32, and as the only difference is with it's memory size, I manually changed the linker command file. It works good.
Ben
Dear Ben
I do not know why different old subjects are being posted here.
Anyway thanks for answering.
Joerg