Hi I am doing a dissertation submitted for a diploma about implementing USB- Host in an embedded system. I have chosen the MCF52223 microcontroller. But I have no idea where to start, so I ask you... is there any example code that could help me understand a little bit? The application I am thinking at is standalone without need of an OS. I should be able to read/write on an USB- memorystick.
I have downloaded this file - can someone please advise how to implement this on the 52223EVB. Am I correct in sayting that this forms the basis of code required for Mass Class Storage for the EVB platform as the host and file transfer to and from the Mem stick.