dear jaux
i am also in your position, i uses freescale cpu exclusively but codewarrior is too expensive and can be complex to use
i am also well versed in forth
but forth inc's swiftx is not user friendly at all and their support is costly as well
although there are already many hcs08 cpu,s they only release a demo for gb60 and
there is no standalone file where you can change the setting to make it work for other cpu's
as i am also thinking of using swiftx to work on hcs08QE cpu, i discovered that i am having difficulty porting
from gb60 to other similar cpu
so that was why i am here because i needed help to do so and i was wondering if it is safe to use swiftx
since forth inc dont even seems to support easy porting on similar cpu ( documentation totally silent on this )
i will try it if i can find good user forum or community support for it
so can you help me in porting the swiftx hcs08 version to hcs08QE cpus
thanks