This problem is still unresolved. Here's an interesting phenomenon that I've discovered:
- Connect a different network device to the WiFi bridge and have it establish contact succesfully.
- Unplug that device from the WiFi bridge
- Configure the NE64 to use the same MAC address as the previous device
- Plug the NE64 into the WiFi bridge
Using this sequence, the NE64 can transmit packets via the WiFi bridge.
So, obviously, there's some initialisation sequence that the NE64 and WiFi bridge do not successfully complete. D-Link (makers of the WiFi bridge) haven't been particularly helpful at explaining what the WiFi bridge does differently than, say, a wired router (which the NE64 CAN communicate with).
Does this give anyone any more ideas of what might be wrong???
Thanks,
Jeff