Hi Luigi
Please go to
http://www.utasker.com/Licensing/License.html to see the licensing terms. Then return the simple application form on that page or here:
http://www.utasker.com/Licensing/License.txtImportant: Please note that we use the application information to help define the best package for your requirement and also as a reference when giving support. No information is made available to third parties or used for advertising etc.
After application (for educational/hobby, evaluation or commercial use as appropriate) you will receive the complete project including source and a powerful simulator. This is set up for CW6.3 on the EVB or DEMO board.
If you would like to simply run the uTasker demo project on your hardware you can freely try this by downloading the target code from the software page:
http://www.utasker.com/software/software.htmlThe default IP address of the board will be 192.168.0.3 and can then be changed and saved via web browser, Telnet or UART. Follow the step-by-step instructions for loading to your board in the Coldfire tutorial:
http://www.utasker.com/docs/M5223X/uTaskerV1.2-Tutorial-M5223X.PDFThe default web pages are also at the software link. You can change them if you wish and simply load them via FTP to the target.
I look forward to hearing from you again.
Regards
Mark