AnsweredAssumed Answered

HC12 project runs in debugger but not standalone

Question asked by Oliver Scholz on Sep 19, 2006
Latest reply on Sep 21, 2006 by MIKE YETSKO
Hi,

I am working with a HC12B32 board we have developed, the application was developed with CW1.0 quite a while ago.

Now I had to make some changes, and I converted the project to CW3.1. It runs great in the debugger with the target connected via the Motorola SDI. But it no longer runs standalone!

In the old compiler I could program the flash with the ABS file and then the board would run without the SDI attached. However, this is no longer the case with CW3.1. Am I doing something wrong? I tried programming the new ABS file with the 1.0 debugger, same effect. The programming runs through without errors, but the board no longer runs. I have no clue what is the cause of this.

Any help would be much appreciated.

Best regards


Oliver

Outcomes