how about the driving capability of REG33V of 908JW32?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how about the driving capability of REG33V of 908JW32?

1,334 Views
jjl3
Contributor I
I can't find the description about this information in the datasheet of MC68HC908JW32.
I want to use it as a 3.3V power supply for a RF IC to save a LDO.
whether can I do as above?
in addition, if I use VDD(5V) as Vtst to connect to pin IRQ of 908jw32, whether can 908jw32 enter monitor mode ?
 
Thanks & best regards
Ji
Labels (1)
0 Kudos
2 Replies

329 Views
jjl3
Contributor I
Thanks Mr ok2ucx a lot!
0 Kudos

329 Views
ok2ucx
Contributor IV
Hallo Ji,
 
HC908JW32's 33VREG pin cannot drive anything external. Its purpose is only for internal power supply for USB. Simple answer is no. I only guess that this voltage might be used just as a reference if you have some power component (OpAmp, transistor) available in you design.
 
To enter the monitor mode of HC908JW32, you need to apply 7.5-8V onto IRQ pin (plus some other logic levels on other pins). 5V is not enough. You may have a look in ZSTAR ref. design (RD3152MMA7260Q) to see what's the monitor mode interface in the real application. Unfortunately there's no default USB bootloader that could be used ;-( So that's why AN2295 bootloader has been adopted for USB with JW32 on ZSTAR.
 
Regards, Pavel ok2ucx
Freescale CZ
 
0 Kudos