Jim Pantera

unstable mc9s08dr32 debug with the usb-ml-12 pod

Discussion created by Jim Pantera on Aug 2, 2006
Latest reply on Aug 3, 2006 by Jim Pantera
reference:
pod is a P&E Multilink usb-ml-12 with rev5.4 software
codewarrior ide version 5.6.1.1506 win-xp

on an existing design i can only sometimes get the jtag emulator to load memory and durn. the nature of the bad is:
-difficult to get code into the processor (mc9s08dr32)
-the crystal is 8mhz difficult to keep it set to this
-sometimes it will run but just setting a break point causes an error

all this on an existing project that functions well in the field.

Outcomes