Gal Afel

ERROR: can't get kernel image!

Discussion created by Gal Afel on Jun 29, 2012

Hello everyone,

 

I'm new to this forum and the Freescale Tower System. I purchased a TWR-MPC8309 with the MPC830x-TLCD a couple of days ago, with the TWR-ELEV and TWR-SER2 modules. When I connect the USB2 Full Speed port to a host computer USB port, the board powers up and it should automatically boot the Freescale Linux OS and run an informational demo showing a JPEG slideshow on the LCD display. However, the OS doesn't boot and instead the following message is shown in the LCD display:

 

Wrong image Format for bootm command 

ERROR: can't get kernel image!

 

I already installed the driver included on the DVD but I can't figure out how to solve this problem.

Any help would be greatly appreciated.

 

Gal Afel

Outcomes