Bitt Sitt

Redpine MQX 3.7 patch doesn't work for Win7-64bit

Discussion created by Bitt Sitt on Apr 13, 2012
Latest reply on Apr 16, 2012 by Bitt Sitt

I only get an error message: "Could not start application" if I try to startit from Windows Explorer.

 

Starting from command line I get error:

This version of C:\Data\Prosjekt\Freescale\FSLMQXOS_3_7_REDPINE_PATCH.exe is not
compatible with the version of Windows you're running. Check your computer's sy
stem information to see whether you need a x86 (32-bit) or x64 (64-bit) version
of the program, and then contact the software publisher.

 

I tried compatibility mode as well to no avail (not sure if I used the right settings though). 

 

Does anybody have a solution for this? Of course a patch for 3.8 (that works) would be even better....

Outcomes