Solved! Go to Solution.
Hello
The simulation issue is not fixed in V5.1 with service pack. But at least with V5.1 and service pack installed you should be able to debug on real hardware.
CrasyCat
Hello
I assume you are using full chip simulation. Am I right?
Full chip simulation for diverse HC08 MCU are missing simulation of KBIPR register.I have already reported that to P&E asking them for a fix.
In the mean time I can only advise you to use the real hardware for debugging.
Also note that the HC908QT4A is only supported with CodeWarrior for HC(S)08 V5.1 after you install the appropriate service pack.
I hope this helps.
CrasyCat
Hello
The simulation issue is not fixed in V5.1 with service pack. But at least with V5.1 and service pack installed you should be able to debug on real hardware.
CrasyCat