Abhishek Roy

programmable pins of MC68HC908QB8

Discussion created by Abhishek Roy on Jun 15, 2006
Latest reply on Jun 19, 2006 by Raghavendra Sorab
Hello
I am using MC68HC908QB8 microcontroller in my project.Can i connect port A of the microcontroller to the programmer.The microcontroller has 16 pins in total.It has 6 pins which are dedicated for multiple purposes(I/O port,A/D channel,Key board interface bits).if notkindly update me on the programmable pins of the QB8 microcontroller.
 
regards
Abhishek

Outcomes