uTasker uTasker

K40 Tower Board SLCD demo and simulation

Discussion created by uTasker uTasker on Jul 22, 2011
Latest reply on Jul 31, 2011 by uTasker uTasker

Hi All

Please note that K40 support has been added for the TWR-K40X256 module, including SLCD controller.

Since these devices are targeted at low power applications where segment LCDs are used (integrated SLCD controller) it was felt important to be able to accelerate developments of such projects by adding an SLCD simulator.

This can now be seen in the follow short video: http://www.youtube.com/watch?v=nm2DmZv1rj8

The video references the user's guide to using the SLCD simulator as well as configuring user defined script files to add any further LCD types, including user-defined ones [this allows users to design their own custom LCDs and complete software development with them before the modules are actually available in hardware] - this document is available at: http://www.utasker.com/docs/uTasker/uTasker_SLCD.pdf

 

Regards

 

Mark

 

www.uTasker.com

Outcomes