Message Edited by rhinoceroshead on 2006-06-08 09:47 AM
ok, found this link http://translate.google.com/translate?u=http%3A%2F%2Fwww.geocities.jp%2Fprogrammer_noritan%2Fhc08%2F...
It looks pretty simple actaully. Just Vss(Ground), Vdd(+), reset and that background debug line does everything. This isnt that much more work for saving $50 plus another development board to play with.
Message Edited by illiterate2006 on 2006-06-08 02:04 PM
Message Edited by illiterate2006 on 2006-06-08 02:05 PM
imajeff wrote:
Converting the $50 board to a BDM is easy, but I only would expect it to
work for the 8-bit MCUs. Anybody tried to load new firmware onto the
on-board UF32?
rhinoceroshead wrote:
Is the HCS08 BDM not the same as the HCS12 one?
Hi,
The P&E USB Multilink in the blue/purple box serves both S08 and S12. The Axiom schematic drawing for the QG board just shows a box with P&E USBBDM for this. It would seem to be not worthwhile to hobble it to restrict it to S08.
When you use one with CW it will reflash it if the firmware is older than what it knows about. So this may S12 enable it anyway.
What is needed is for somebody to "give it a go" and let us know.
Regards David
Message Edited by peg on 2006-06-10 11:52 AM
peg wrote: Hi,The P&E USB Multilink in the blue/purple box serves both S08 and S12. The Axiom schematic drawing for the QG board just shows a box with P&E USBBDM for this. It would seem to be not worthwhile to hobble it to restrict it to S08.
Hi Rhino,
Yes, it does it automatically via the P&E Micro flash programmer interface.
Cheers,
Alban.
Hi,
TOO automatically for my liking!
I had been using my USB Multilink for many months with P&E software then when I first used it with a fresh install of CW5 it just did it without asking me or even advising me. It all happened in a few seconds just flashed up a screen that it was doing it then the screen dissappeared. If I had looked away I would not have even known. My main issue with this was if it had introduced some problem I would not have known to blame the update first.
Regards David