I have programmed and debuged on processor PC9S12XDP512MFV QL15Y QZXH0536 with Codewarrior 4.1 and my program works fine, but now when I try to flash PC9S12XDP512MFV C66151.12 OL40V QZAH0428 my program doesn't start! What should I change in the project!
When I try to run the program in Real-Time Debugger I get an error saying "Other BGND 524D" ILLEGAL_BP What does that mean?
thanks in advance Patrik
Message Edited by Alban on 06-06-2006 02:07 PM
Hello
Send me y private message with your email address and I will upload the web installer on FTP for you.
CrasyCat
Patrik,
You said it worked before, does the 4.5 debugger talk to the L40V? If so I'd guess that there's maybe a newer P&E driver or something.
I don't recommend using L40V - I'm assuming in this case that there is no other choice. The silicon isn't qualified and is missing a bunch of features and fixes that L15Y has.
Alban wrote:
Euh, I'm sorry but you should NOT develop on L40V.
Message Edited by imajeff on 06-06-2006 08:14 AM
Patrik, a similar problem was posted in another thread. I'll repost my answer here. There are some important differences between the two masksets so it is likely your code will not work directly on both masksets