yuxing yao

Support files for MCF5225X and Connector for TWR system

Discussion created by yuxing yao on Jun 21, 2011
Latest reply on Jul 6, 2011 by Michael Norman

Hi there,

 

I recently migrated to Freescale tower system.

 

Current environment: TWR with MCF5225X in CodeWarrior 10.1

Old environment: MCF5211DEMO board in CodeWarriror 5.7.0

 

In the old dev environment when a new project is created, CodeWarrior would have a set of support files available, like mcf5xxx.c, mcf5xxx_lo.s, which contains some support functions like cpu_pause(), asm_set_ipl(), mcf5xxx_set_handler(), etc. 

 

So my question is, are there any similar files/functions that are available in CW10.1?

 

I do have the source code so I assume copying them over could solve my problem, but I would like to have CW10.1 make it a bundle when creating new projects.

 

Thanks in advance.

Outcomes