Hi Nicholas,
I don't really know what you have, but....
The GT60 is really a GB60 with less pins so for the purpose of the SMAC (which uses the SPI and a few pins) the code to run this will be the same for both.
Regards David
Hi nico,
I have SMAC4.1a and two 13192-SARD boards which use GT60. I have downloaded and run all the examples on my boards successfully so no, I don't know your problem.
Regards David
Hi nico,
If you are using SARD boards the library is:
SMAC_13192sard_4_1a.lib
If you open an example its under the SMAC section in the project pane.
It is located in: \SMAC4.1a\S08\smac\3.1\bin
The source for it is: \SMAC4.1a\SMAC(Sources)
You have to find where the functions are used within the supplied examples yourself.
Hope this helps,
Regards David
Thanks !
I can use the funcction now.
I made this program :
Code:
for(;;) { UINT8 MLMESetChannelRequest(UINT8 u3Channel); UINT8 MCPSDataRequest(tTxPacket *psTxPacket); UINT8 MLMESetChannelRequest(UINT8 u12Channel); UINT8 MLMERXEnableRequest(tRxPacket *psRxPacket, UINT32 u32Timeout);}
I want to receive and send data, but with this function, nothing sent and received
How use this function to send datas (bacon)?
Thanks
Nico
(Alban formatted code)
Message Edited by Alban on 2006-06-07 11:04 AM