Had problems - cannot replace dbug with Colilo from v2.6 LTIB BSP (200512xx.iso)
TARGET Board: M5474Lite (M5475AFE); recognized there is no NOR flash and no code flash. Colilo must be in Boot Flash to replace dbug...
tried using dbug to load colilo_mcf5475.srec (tried both rebuilt on host and using the srec from the bsp '/images' directory) to RAM area first (go colilo at 1000400) and successfully saw a
colilo>
prompt came up, then tried to tftp colilo_mcf5475_only.bin to boot flash (image size = 65258 bytes) and flash 0xff800000 0x1000, then go 0xff800400 and saw a couple of weird characters before the lines of "Colilo M547x-M548x Bootloader" and "2005 Freescale/2004 Motorola (c)" came up. Then supposingly I reset the board and should see colilo come up after reset, but failed.
please see some other issues as in attachments