Very nice demo, nice looking product and application, and thank you for supporting Freescale microcontrollers!
I've forwarded your post to many within Freescale.
Regards, DavidS
Hi DavidS
Thanks indeed.
Anyone with the M5223XEVB or the DEMO board can try out the uTasker demo project on their own board by loading the following file
http://www.mjbc.ch/software/uTasker/M5223X/uTaskerV1.2beta005_m5223X.s19
It can be downloaded to the M5223XEVB/DEMO board using CF Flasher V3.1.1 (free Flasher from freescale) (make sure the newest version is used!!)
The default IP address is 192.168.0.3 and it supports web, ftp, Telnet and SMTP (SMTP test will however try to use my provider so will fail…). The settings can then be modified via Telnet or via web browser once the web sides are loaded.
To load the web pages, copy them from the on-line demo at ftp://212.254.22.36/ and then load them to your local board, also using FTP. Use IE6 in non-passive mode and drag-and-drop from the on-line demo directly to the local board should be possible.
The demo project can be completely simulated using the uTasker simulator (in real-time on a real network). Don't forget that educational and hobby use of the uTasker is completely free, including email support and regular newsletters.
uTasker projects run on the NE64 or the M5223X - simple set one compiler switch and compile for the target of your choice!!
Regards
Mark Butcher
www.mjbc.ch