Erich Styger

CW 10.1 for TWR-LCD and MCF51CN128

Discussion created by Erich Styger on Mar 19, 2011

Hello,

I have finally ported my Processor Expert to MCU10.1 with all the components. Now it includes as well the USB bootloader as component :-).

The archive contains 3 projects: one for the MCF51CN128, one for the TWR-LCD MCF51JM128 both as standalone and with bootloader enabled, and one project to build the USB bootloader. The archive contains a documentation pdf which should give you more information, and the needed Processor Expert components are inside the TWR-LCD JM128 project as *.PEupd file.

 

Features:

- nearly everything made from components, so you can graphically configure the software

- USB bootloader, FatFS SD card driver, FreeRTOS operating system, ...

- Graphical UI (screen, window, dialog, buttons, lines, graphs, fonts, text, drop down boxes, check boxes, calendar view, ...)

- Button and navigation switch support, as well routing navigation switch messages from the JM128 to the CN128

- UI demo with accelerometer changing the screen at runtime (CN128), touchscreen calibration, RTOS task list, 3D graphic demo, ...

 

Have fun :-)

Erich

Original Attachment has been moved to: 143-TWRLCDMCU10.1.zip

Outcomes