Hi,
I want to know if someone had success with the flash_over_jtag application?
I’m using flash_over_jtag_v2.exe and 568346_flash.cfg that came when I installed CodeWarrior 7.1 and updated at 7.2.
I don’t have the flash config file for the 568345 but the 568346 is the closest I have.
When flash_over_jtag is executed, the mass erase perform well. But I get a CRC on flash #0 (program flash) after it’s programmed.
Can someone give me a hint on this one?
Regards
Steel
The DSC 8.1 is a patch for the DSC8.0 (must be installed in first)
You can download this version on our web site via the link:
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600617882140B
Pascal