Brad Anthony

Problem connecting to JM60

Discussion created by Brad Anthony on Nov 7, 2010
Latest reply on Nov 8, 2010 by Derek Snell
We are currently working with the PCF51CN128 and have been unable to successfully program the board.  It is hooked up to a windows 7 x86 laptop that is running CodeWarrior 10 and MXQ 3.6.1.  We have been testing with the security web server sample that is provided with the MQX RTOS.  We get this error message when trying to connect to the board.  "Launching Test_connect has encountered a problem.  ColdFire GDI Protocol Adapter: Can't connect.  The Debugger can not connect to OSBDM."  It is configured using OSBDM-JM60 ColdFire V1.

My questions are:  Is this a windows 7 driver issue, or is it a misconfiguration of Code Warrior?  Can it be a firmware version problem with the JM60 unit on the board?

Attachments

Outcomes