Background info:
My Tech.Arts(T.A) adapt9s12e128 eval board has (b) in it, but that may be programmed by T.A.
The TA Adapt9s12e128 documentation section 3.9 says "Since the 2k serial monitor is included on chip..".
The mc9s12e128(p99 sec10) and mc9s12a128(p88 sec17) Device User Guides say - "It is planned that most devices made after Q1 of 2004 will be shipped with the LRAE " which is option (a) above.
Obviously I should look at a new chips memory, when I get one, but for now it would be a great help if someone could say if a or b above applies.
Message Edited by bobz on 04-19-200601:58 PM
Thats great thanks, using bdm was always 'plan A' anyway for initial programming. Now we know the flash is blank we know bdm is the only option for initial programming which is fine since a bdm connector will be fitted on our board and we were never considering not having a bdm programmer.
I was mostly interested in whether the monitor was pre-programmed because it's excellent. It seemed wise to take advantage of it ASAP once I could get a handle on whether or not it was there from the start and how likely that flash is to change.
Secondly, once on the board, I was interested in simple but safe ways of utilizing the monitor from the application so that the application could use the serial port for itself and for reprogramming the application in flash.
The obvious solution is to learn from the dbug12 monitor code and the various associated app notes on the www.freescale.com and www.Technologicalarts.ca websites.
Thanks again.