David Myers

GB32 Real Time Interrupt

Discussion created by David Myers on Apr 18, 2006
Latest reply on Jun 8, 2006 by Gabriel Sanchez Barba

I am trying to use the real-time interrupt on the GB32 but the interrupt never arrives when the circuit board is connected to the BDM and the true time simulator. If the circuit board is not connected to the BDM the interrupt works exactly as I think it should. The problem is that I can't debug the code without the BDM.

Is there a problem with entering stop mode or with the internal oscillator while connected to the BDM?

Thanks,

Binst

Outcomes