Hello,
This issue is really addressed to Freescale, but if others can throw light on the situation, I would welcome any comments.
I refer to Revision 3 of AN1831 (Nov 2005), and the programmming of flash for storage of non-volatile data within an application, for QT/QT devices specifically. I make the following observations with the revised AN.
- The AN makes no differentiation between the older (classic) devices, and the newer (A-suffix) devices. In fact it makes no specific mention of the latter.
- It states that the "page erase" issue does not apply to QT/QY devices. But when using the PRGRNGE routine, row boundaries must now not be crossed, for the QT/QY devices only.
- It is stated numerously that the QT/QY devices now only support 1 MHz bus frequency for erase or programming operations (with CPUSPD = 4).
If my observations are correct, this seems to be "shifting the goal posts" somewhat, from the previous situation.
I currently do use the ROM-based routines in a number of applications, for page erase and for programming of classic devices only. I have been doing so (successfully) for the last two years or so, using the internal oscillator (bus clock = 3.2 MHz), and CPUSPD = 13. So the following questions arise -
- Do the new limitations apply to both classic and A-suffix devices? If so, when did this take effect, and how do I recognize whether a batch of devices will have the new limitations, or not? The mask set ID does not currently appear on any of the pieces within my stock (only a date code).
- For my existing applications, do I need to modify my usage to reflect these changes (assuming continued use of the classic devices) - perhaps to implement my own routines?
- Of particular concern is the lowering of the maximum bus rate to accommodate erase and programming. Since the classic device does not have a 1 MHz bus option, does this imply that an external 4 MHz crystal/oscillator must now be used where flash programming within an application is required? What would be the likely effect of continuing to use the 3.2 MHz bus rate (with CPUSPD = 13)?
Of course, if the additional limitations (and the Application Note) apply only to the new A-suffix devices, does there still remain a "page erase" issue for the classic devices (as there once was)?
Thank you in anticipation.
Regards,
Mac