Hi,
I am trying to program MCF52259 demo kit micro controller. At the moment I am stuck with USB Endpoint 0. When I connect my usb, I get interrupt and then asked for Get_Descriptor. I send the device descriptor then it resets but after resetting, it again asks for device descriptor instead of issuing Set_Address command.
What could be the cause of the problem.
Here is the sequence of events that I encountered.
RESET
SETUP - Get_Descritpor
IN
OUT
RESET
SETUP - Get_Descritpor
IN
OUT
RESET
SETUP - Get_Descritpor
IN
OUT
Hello,
maybe you have a problem with overlapping Interrupt Priorities.
Have a look at this http://mcuoneclipse.wordpress.com/2012/04/22/trapspitfalls-overlapping-interrupt-priorities/
Eckhard
Thanks for the reply.
I checked all the interrupt handlers. I am not receiving any interrupt apart from USB.
But still I am getting the same problem.
I looked into the sample programs on the internet but can't find whats the problem.
Any help will be highly appreciated.
Regards.
Hello,
try using a software usb sniffer for detail packet transfer.
find whose creating problem 1)is it PC who cannot detect ACK signals from MCF52259
2) Or device which cannot send descriptor in required format.
Swapnil.