OSBDM Connection error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OSBDM Connection error

454 Views
quevedo
Contributor V

Hello,

 

I am having problems connecting CW10.2 with my Tower board. I have a TWR-SENSOR board, with an embedded OSBDM. I have already updated its firmware to the latest version, and the drivers for OSBDM and CDC were installed with no problem at all.

 

When I try to enter debug mode and load my program into the S08QE96 onboard processor, I get the attached error message. Nothing that I have tried to do has worked. I have tried to connect this board with two different computers (one with 32-bit WinXP, other with 64-bit Win7), and the message is the same for both.

 

Any ideas on what can be going on?

 

Thanks in advance

Tags (2)
0 Kudos
0 Replies