AnsweredAssumed Answered

TWR K60 ADC1_DM1 and ADC1_DP1

Question asked by DALE RODDA on Aug 9, 2012
Latest reply on Aug 9, 2012 by Mark Butcher

Looking at the schematic for the K60 tower there is a pot with the wiper labeled ADC1_DM1 which is connected to a pin labeled K2. Searching through the source files show that int_gpio.c is channel 20. This matches up to ADC_Task.c. I want to use ADC1_DP1 which goes from K1 to the on of the touch pad connector U2. I can not find a channel associated with ADC1_DP1. 

Does anyone know which channel ADC1_DP1 is or where I can find out?

 

Thanks

Outcomes