Solved! Go to Solution.
Hello
I was asking as the answer is different for HC08, HC12, Coldfire, or PPC :smileyhappy:
The description below is valid for HC08 & Hc12, HCS12.
If you are using HC08 tools there is a CHECKSUM command that you can use in the linker .prm file.
For information how to use that command look in the Linker manual. There is a description of the command CHECKSUM in there.
You can also find some example project using the CHECKSUM command in the {Install}\(CodeWarrior_Examples)\HC08\Checksums directory for HC08 and
{Install}\(CodeWarrior_Examples)\HC12\Checksums for HC12.
I hope this helps.
CrasyCat
Hello
I was asking as the answer is different for HC08, HC12, Coldfire, or PPC :smileyhappy:
The description below is valid for HC08 & Hc12, HCS12.
If you are using HC08 tools there is a CHECKSUM command that you can use in the linker .prm file.
For information how to use that command look in the Linker manual. There is a description of the command CHECKSUM in there.
You can also find some example project using the CHECKSUM command in the {Install}\(CodeWarrior_Examples)\HC08\Checksums directory for HC08 and
{Install}\(CodeWarrior_Examples)\HC12\Checksums for HC12.
I hope this helps.
CrasyCat
CHECKSUM CHECKSUM_ENTRY METHOD_CRC16 OF READ_ONLY 0xE000 TO 0xFBFF INTO READ_ONLY 0xFF70 SIZE 2 UNDEFINED 0xFF ENDEND
Hello
Which processor are you targeting (HC08, MPC, ...)?
CrasyCat