Hi
A colleague has created a QCS project and used the DPAA Graphing Tool to create a DPAA configuration. Here are the project's directory contents:
MyProj_DPAA/
├── .cproject
├── .cwGeneratedFileSetLog
├── Documentation
│ ├── ProcessorExpert_Settings.previous.xml
│ ├── ProcessorExpert_Settings.xml
│ ├── ProcessorExpert_SIGNALS.txt
│ └── ProcessorExpert.txt
├── Generated_Code
│ └── DPAA1
│ ├── dpc_struct.h
│ ├── fmc_config.c
│ ├── fmc_config.xml
│ ├── fmc_dpc.xml
│ ├── fmc_pcd.xml
│ └── .log.txt
├── .ProcessorExpert.g_c
├── .ProcessorExpert.g_x
├── ProcessorExpert.pe
├── .project
├── .settings
│ └── com.processorexpert.core.ide.newprojectwizard.prefs
└── Sources
└── DPAA1_SWParser.xml
I have two questions:
1) I want to store this project in Subversion. Which files do I need to version control? (For a C/C++ Eclipse project I would version control .project, .cproject and the source files).
2) How can I import this project into my own workspace?
Best regards
David
Solved! Go to Solution.
Hi,
ad 1) It depends if you want to version also the generated output files. However, minimum files for QCS tools project re-generation are ProcessorExpert.pe and "Sources" directory with content. You need also eclipse project files, I'm not sure what are all of them (.project, .cproject etc.)
You can delete Documentation, Generated_Code and .ProcessorExpert.g* and these files will automatically be re-gerated after new code generation.
ad 2) You can use a menu command File > Import... , select General / Existing project into Workspace..., then select root directory of the project or archive file.
best regards
Petr Hradsky
Processor Expert Support Team
Hi,
ad 1) It depends if you want to version also the generated output files. However, minimum files for QCS tools project re-generation are ProcessorExpert.pe and "Sources" directory with content. You need also eclipse project files, I'm not sure what are all of them (.project, .cproject etc.)
You can delete Documentation, Generated_Code and .ProcessorExpert.g* and these files will automatically be re-gerated after new code generation.
ad 2) You can use a menu command File > Import... , select General / Existing project into Workspace..., then select root directory of the project or archive file.
best regards
Petr Hradsky
Processor Expert Support Team