I am on my first day with CW for the K70 tower. I have been able to rebuild the MQX libs (195 warnings, mostly pragmas) . The debug versions were built. Is it necessary to rebuild the release versions as well? If so.. do I just change the target for each of the imported libs and rebuild all ? UPDATE: found this answer in docs..
Also.. I had attempted to imnport the working set as per the instructions but no sets were imported. Dragging the wsd file into the CW workspace only opened up the file. Normal?
Solved! Go to Solution.
Pleas make sure, that you have MQX plug-ins for CodeWarrior correctly installed. You may figure it out in the following way:
- go to Help/About CodeWarrior Development Studio menu
- click the "Installation Details" button
- go to the "Plug-ins" tab and sort plugins by ID
- check if you have the plug-in wiht "com.freescale.projectofprojects" ID (see the attached screenshot)
If you don't have this plug-ins installed (the other reason is that wsd file is corrupted, what shouldn't be the case), go to the <MQX installation path>\tools\codewarrior_extensions\CW MCU v10.2\ folder and you may install plug-ins using the "install_cw10.2_plugin.bat" script, however be careful, because there is a bug in CodeWarrior which corrupts the debugger in some way, to avoid it you should replace scripts (un-/install_cw10.2_plugin.bat) with the ones form this archive: Zip .In other words: first update scripts then install plug-ins.
Best Regars,
Marcin
Hello crezyoz,
I assume you are using CW 10.1 which does not have all functionalities to import the working set. This working set is fully fucntional in CW10.2.
Regards,
MartinK
I am using 10.2
Pleas make sure, that you have MQX plug-ins for CodeWarrior correctly installed. You may figure it out in the following way:
- go to Help/About CodeWarrior Development Studio menu
- click the "Installation Details" button
- go to the "Plug-ins" tab and sort plugins by ID
- check if you have the plug-in wiht "com.freescale.projectofprojects" ID (see the attached screenshot)
If you don't have this plug-ins installed (the other reason is that wsd file is corrupted, what shouldn't be the case), go to the <MQX installation path>\tools\codewarrior_extensions\CW MCU v10.2\ folder and you may install plug-ins using the "install_cw10.2_plugin.bat" script, however be careful, because there is a bug in CodeWarrior which corrupts the debugger in some way, to avoid it you should replace scripts (un-/install_cw10.2_plugin.bat) with the ones form this archive: Zip .In other words: first update scripts then install plug-ins.
Best Regars,
Marcin
Thank you Marcin.