K10. Uart rx-Irq stopped at baud-s higher then 230400

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K10. Uart rx-Irq stopped at baud-s higher then 230400

570 Views
tty
Contributor I

When I communicate at second uart with high speed (460800 and 921600) between two kinetis K10 I see RX-IRQ stopped after some time-lapse.  On other speeds all works well.

1) I'm using the kuart MQX driver (3.8) in interrupt mode and I configured it for this speed.

2) I'm using a 40MHz crystal and 40MHz  sys bus.

 

What is this might be?

 

Thanks a lot.

0 Kudos
1 Reply

368 Views
Xlerb
Contributor II

Hi tty,

May not be the source of your problem but the K10 is only supposed to work with crystals up to 32MHz.

Cheers,

Martin.

0 Kudos