AnsweredAssumed Answered

Can CW 6.3 Be Tricked Into Supporting MCF51MMxx parts?

Question asked by Wade Hassler on Jun 3, 2012
Latest reply on Jun 4, 2012 by kef

.... the reason I ask is that I have a 64-bit Windows machine, on which CodeWarrior 6.3's Installer will not run.(I have Windows 7 Home version, which Microsoft claims cannot be forced to load Xp programs.)

If CW is installed on a removable drive that is attached to a 32-bit Windows machine, it works just fine when moved to a 64-bit machine.

So far, so good. Now I want to test-drive an MCF51MMxx, which is not supported by the CW6.3 that I have.

Do I have to go through all the same hooha again, or are there data-files supporting the MM-parts that can be added to the existing installation?

 

Wade Hassler

Outcomes