RICK BOURGEOIS

MCF52259 RTC speeds up during BWDT reset

Discussion created by RICK BOURGEOIS on May 29, 2012
Latest reply on May 31, 2012 by RICK BOURGEOIS

I am using MQX VERSION 3.6 for my custom designed board with a MCF52259. I have recently added a Backup Watch Dog Timer to the code. The BWDT has been introduced because static electricity can cause the program to crash or the ethernet phy chip to crash. The BWDT kicks in whenever I loose communications up to two times in a row.

 

My testing department claims that the clock is gaining two seconds every time the BWDT resets the board.

For my application I cannot allow the clock to drift more than 30 seconds in a day. At night the clock is automatically re-synched.

I am using MQX generated code to initialize the RTC.

Has anyone out there ever experienced this problem?

 

Outcomes